This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Coefficient update --- using poles and zeroes



 fs=100000; //16Khz
   fz1=2000;
 fz2=(fs/3.14);
 fp2=(fs/3.14);
 fp1=0;
 Kdc=6000;
 pi=3.14;

 

// Coefficient update --- using poles and zeroes
    wz1 = 2*pi*fz1;
 wz2 = 2*pi*fz2;
 wp1 = 0; //Integrator pole at f=0
 wp2 = 2*pi*fp2;
 
 wr = sqrt(wz1*wz2);
 Q = wz1*wz2/((wz1+wz2)*wr);
 
 c2 = Kdc/(wr*wr);
 c1 = Kdc/(Q*wr);
 c0 = Kdc;
 
 d2 = 1/wp2;
 d1 = 1;
 d0 = 0;
 
 den =  4*d2*fs*fs + 2*d1*fs + d0;
 
 B0_I = (4*c2*fs*fs + 2*c1*fs + c0)/den;
 B1_I = (-8*c2*fs*fs           + 2*c0)/den;
 B2_I = (4*c2*fs*fs - 2*c1*fs + c0)/den;
 
 A1_I = ((-8*d2*fs*fs           + 2*d0)/den)*-1.0;
 A2_I = ((4*d2*fs*fs - 2*d1*fs + d0)/den)*-1.0;
 
 CNTL_2P2Z_CLACoefStruct2.b2   =B2_I;  // B2
    CNTL_2P2Z_CLACoefStruct2.b1   =B1_I;  // B1
    CNTL_2P2Z_CLACoefStruct2.b0   =B0_I;  // B0
    CNTL_2P2Z_CLACoefStruct2.a2   =A2_I;  // A2
    CNTL_2P2Z_CLACoefStruct2.a1   =A1_I;  // A1 
    CNTL_2P2Z_CLACoefStruct2.max  =Dmax_I;//Clamp Hi
    CNTL_2P2Z_CLACoefStruct2.min  =0.0;   //Clamp Min

 

请教一下,二阶系统的系数是怎么确定的??