This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于28031复位期间,GPIO输出幅值为1V,时间为复位时间脉冲的问题



大家好!

        我在使用28031 PN型号(即80pin的芯片),VREG功能不使能,我外加了一个复位电路,复位时间为200ms,这时发现每当复位时,GPIO口都会输出一个200ms 幅值为 1V左右的脉冲。

        我将外部复位电路断开,由于其内部有  POR  复位电路,DSP仍能上电工作,但是这个脉冲仍然出现,只是时间变为几个ms,我查看了POR的复位时间为400~800us,不知为何会出现种情况?

        另外,我将3.3V与1.8V电源的上电时序反复调整,即1.8V超前3.3V或者3.3V超前1.8V,均不能解决这个问题。当1.8V先上电时,3.3V缓慢上升过程中,GPIO的输出也会缓慢上升,当3.3V上升到2.8V时,GPIO会突然变为低电平(这是所期望的上电输出状态)。

     我希望DSP的GPIO口在上电时像2808或28016一样输出低电平,不希望有这个脉冲出现,请问大家该怎么解决这个问题啊?谢谢!