This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS100V2仿真器连接问题



我的目标板为 F28035

软件 CCS4.2.4

仿真器有两款

XDS100V1  为XDS100的版本 V1

XDS100V2  为XDS100的版本 V2

当目标板采用XDS100V1时,可以连起可以仿真,

当目标板采用XDS100V2时,无法连起。

  • 楼主是否在target configuration 中,有设置仿真器为XDS100V2?

  • 楼主用的是哪个公司的XDS100V2?

    所谓不能连接,是指不能启动在target configuration中的XDS100V2,(target configuration 中设置好后鼠标右键lanuch)

                 还是指启动XDS100V2后不能connect(lannch后CCS->target-->connect)

    前者可能是仿真器驱动,或者就是仿真器有问题。

    后者可能是仿真器到开发板的JTAG通路有问题,既然谈到“当目标板采用XDS100V1时,可以连起可以仿真"那估计是仿真器这边有问题。

  •    是这样的, 不能连接是,我点connect 后,会报错。不能连接

     连接XDS100V2的时候,我当然配置了仿真器类型。选的是XDS100V2。

     如果说XDS100V2仿真器的问题,但它连接 F28335 的时候是可以很好的连接起的,

     我想问的是,XDS100V2跟XDS100V1有什么区别,为什么一个不能连接一个能连接?  

  • XDS100V2和V1在这方面并没有区别,都应可以连接28035和28335。我在这里用TI的28035 Experimenter Kits,一切正常。

    楼主谈到的用的28035的XDS100V1是板载仿真器吧,请确认XDS100V2到28035的通路,板载仿真器是否和XDS100V2冲突。