This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

定点型DSP28027使用IQmath,怎么提高运算效率?

我想请教一下,使用定点型DSP,如果操作数都是整型的,这种情况下,使用普通乘法“ * ”、除法“ / ”和使用_IQNmpy、_IQNdiv哪个执行时间更短,效率更高?

本人测试了一下,发现使用IQmath的执行时间要比相应的普通乘法“ * ”、除法“ / ”的执行时间长的多,我的测试代码如下:

long w,x,y,z;

GpioDataRegs.GPBSET.bit.GPIO32 = 1;

w=_IQ12div(_IQ12(100),_IQ12(9));

x=_IQ12mpy(_IQ12(100),_IQ12(9));

GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1;

GpioDataRegs.GPBSET.bit.GPIO33 = 1;

y=100 / 9;

z=100 * 9;

GpioDataRegs.GPBCLEAR.bit.GPIO33 = 1;

然后,使用示波器观察GPIO32和GPIO33的高电平的时间,结果显示使用IQmath的执行时间要长的多,那么请问,IQmath在什么情况下,才会相对于普通算法而提高效率?(当然了,使用IQmath的结果精度要高)

通道1测试GPIO32,通道2测试GPIO33

谢谢