This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TMS320F240在CCS V3.3用SEED的560下载程序的方法
你好,
The XDS560v2 System Trace unit is fully compatible with TI’s Code Composer Studio™ IDE version 4.2 and newer.
560只支持CCS V4.2以上的版本,建议使用V5以上版本
链接是关于560的详细介绍和相关文档:http://www.ti.com.cn/tool/cn/XDS560
纠正一下上面的错误,560在需要使用系统跟踪功能是只能使用V4.2以上的CCS,基本的仿真和调试支持3.3,附件是seed XDS560在3.3下的使用指南,可供参考。
你好!目前不用调试TMS320F240,只在那个CCS环境下用SEED 560进行程序下载.
因为目前我们用的TMS320F28335是CCS V3.3下进行仿真和调试的,现在公司有需要更换的老板是用TMS320F240芯片,我用CCS V3.3不能下载程序,工具是SEED 560,请指点怎样下载TMS320F240的Flash
可以参考上面的附件,下载程序使用CCS也需要进行必要的几个步骤,先安装560 CCS3.3的驱动,然后在setup中配置仿真器和芯片,并进行设置,最后打开CCS主界面,连上仿真器就可以下载程序了。
你到底有没有有过TMS320F240这个芯片,你说点我不知道的资料好吧!我都和你说过了,我们现在用TMS320F28335用CCS 3.3仿真和调试以及下载是没有问题的,是TMS320F240是用什么软件下载的。
F240已停产多年,没用过很正常。至于560仿真器是否能支持F240, 你应该去找仿真器厂家的资料。
附件是找到了关于F240烧写的资料,希望对你有帮助。
Eric
你好,谁有Flasher-C2000的下载,发一个给我,谢谢!
可以用闻亭泰科的TDS510PLUS,带有烧写软件,按照说明书,选择器件和擦除扇区,选中CCS生成的.out文件烧写即可。我曾购买过一个TDS510PLUS,目前已使用了三年多,尚未出现问题。