我在提高ADC精度的手册中看到图中的方法,所以想问可不可以用芯片自身提供的2V和1V电压?如果不可以,那么这两个引脚有什么作用?如果可以,需要注意什么?手册中有写到ADCREFP和ADCREFM也可以作为输入引脚,作为输入引脚的作用是什么?跟外部基准有什么关系?还有内部基准又是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在提高ADC精度的手册中看到图中的方法,所以想问可不可以用芯片自身提供的2V和1V电压?如果不可以,那么这两个引脚有什么作用?如果可以,需要注意什么?手册中有写到ADCREFP和ADCREFM也可以作为输入引脚,作为输入引脚的作用是什么?跟外部基准有什么关系?还有内部基准又是什么?
图中的意思是给ADC模块提供两路已知电压的输入,通过ADC转化得到的 数字量用于计算线性偏差,这两路电压只需要不相同并不一定是外部参考电压,对吗?简便起见可以直接用外部参考电压,是吗?还是我没有理解你所说的参考电压的意思?首先满量程的3V是一个参考电压,似乎芯片里用到的是一个1V,一个2V作为了参考电压;而另外一种参考电压是指在提高ADC精度的过程中需要两路已知的电压信号,是这样吗?或者说如果我想已知电压对未知电压转化后的数值进行修正的话是不是可以有两种办法呢?第一是采用外部提供参考电压的同时利用外部参考电压作为已知电压;另一种方法是采用内部的参考电压,并且将内部的参考电压引出输入到ADC通道?如图中所示。
你的意思是,用作参考电压的电压做好不要用于作为误差补偿用电压,以免两路电压产生干扰?顺便想多问一下,针对电源干扰的问题,需要将芯片中不同的电源进行隔离,比如,Datasheet中说将VDDA1/2,AVDDREFBG与数字电源进行隔离,那么怎么样才能做到隔离呢?本来我的理解是需要前者和后者电源不共地,但是我又想如果不共地可能ADC模块不能工作(内部电路应该是需要共地的),后来在一些F2812的原理图中看到有通过磁珠进行电源隔离的,不知道这样的隔离效果怎样?还有就是如果采用外部供电,那么这个电压信号怎么与其他的电源信号进行隔离呢?