This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28335中SCI的FIFO使用



接收器的FIFO:在手册里面说的是接收FIFO的中断产生条件是the FIFO status bits (RXFFST4−0) and FIFO level bits (RXFFIL4−0) match (i.e., are greater than or equal to). 也就是说假如我设置(RXFFST4−0)此位为6,那么当SCI接收到6个字节以后才会产生一个中断,对么?但是我在使用发现和我所理解的不一样,它依然是每接受一个字节就进入一次接收中断。