This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335编译器的问题



编译器里面有个编译选项Allow reassociation of FP arithmetic   --fp_reassoc

是干什么用的 编译快速浮点库的时候有开启

  • 你好,这跟浮点库没有关系,用于编译器在编译代码时决定是否关联浮点算法。请参考以下说明:

    --fp_reassoc={on|off}

    Enables or disables the reassociation of floating-point arithmetic. The
    default value is --fp_reassoc=on.
    Because floating-point values are of limited precision, and because
    floating-point operations round, floating-point arithmetic is neither
    associative nor distributive. For instance, (1 + 3e100) - 3e100 is not
    equal to 1 + (3e100 - 3e100). If strictly following IEEE 754, the
    compiler cannot, in general, reassociate floating-point operations.
    Using --fp_reassoc=on allows the compiler to perform the algebraic
    reassociation, at the cost of a small amount of precision for some
    operations.
    When --fp_reassoc=on, RPT MACF32 instructions may be generated.
    Because the RPT MACF32 instruction computes two partial sums and
    adds them together afterward to compute the entire accumulation, the
    result can vary in precision from a serial floating-point multiply
    accumulate loop.