本人在使用CCS4软件时,用了自己买的TDS510仿真器,但是在CCS4进行配置时,发现里面的驱动没有TDS510,所以想在此请教下,如何将TDS510驱动加入到CCS4的驱动文件中。
程序配置在RAM和flash中的区别是什么?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
本人在使用CCS4软件时,用了自己买的TDS510仿真器,但是在CCS4进行配置时,发现里面的驱动没有TDS510,所以想在此请教下,如何将TDS510驱动加入到CCS4的驱动文件中。
程序配置在RAM和flash中的区别是什么?
谢谢!
为什么有时 BOOT_RSVD : origin = 0x000000, length = 0x000050 放在PAGE0里,有时放在PAGE1里?
关于第一个问题,如果指的是PIE vector在DSP2833x_Headers_nonBIOS.cmd中;至于你说的 VECTORS/* part of boot ROM */是BOOT ROM的一部分,具体请看Boot ROM guide
关于第二个问题,没有区别,它只是保留区域,上面有写说明,请看一下:
/* BOOT_RSVD is used by the boot ROM for stack. */
/* This section is only reserved to keep the BOOT ROM from */
/* corrupting this area during the debug process */