我在ccs6.0 28335工程里面没有添加#include<stdlib.h>
为什么当程序里面用到里面的函数的时候能识别且编译通过
iqmath.h 里面的#include<stdlib.h> 已经注释起来了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在ccs6.0 28335工程里面没有添加#include<stdlib.h>
为什么当程序里面用到里面的函数的时候能识别且编译通过
iqmath.h 里面的#include<stdlib.h> 已经注释起来了
事情是这样的 我添加的函数是 abs() 还有 labs();
/* NOTE - Normally, abs, labs, and fabs are expanded inline, so */
/* no formal definition is really required. However, ANSI */
/* requires that they exist as separate functions, so */
/* they are supplied in the library. The prototype is */
/* here mainly for documentation. */
然后这是我f3之后的说明
工程里面绝对不可能有添加头文件所有的文件都是我自己添加的 我最清楚
只是上面的英文说得不是很明白 谁能解释下
或者在自己的工程里面应用一下