This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我想采用定时器10kHz起动AD中断,280x与2812在这方面操作不太一样。请问1:用cputimer0的话,目前的问题是ConfigCpuTimer(&CpuTimer0,100,100); 时间计算的不对,不知道为什么 问2:采用其它定时器的话,怎样操作,280x的比较复杂 谢谢!
楼主看一下ConfigCpuTimer程序吧。
其他定时器一样操作。
void ConfigCpuTimer(struct CPUTIMER_VARS *Timer, float Freq, float Period)
{
Uint32 temp;
Timer->CPUFreqInMHz = Freq; //写入当前CPU的频率
Timer->PeriodInUSec = Period; //写入定时器的周期时间(uS为单位)
temp = (long) (Freq * Period); //计算出需要设定的timer的周期数值
Timer->RegsAddr->PRD.all = temp; //设置CpuTimerx的周期值
Timer->RegsAddr->TPR.all = 0; //不进行分频,即TIM的递减速度等于SYSCLKOUT
Timer->RegsAddr->TPRH.all = 0;
Timer->RegsAddr->TCR.bit.TSS = 1; //停止计数
Timer->RegsAddr->TCR.bit.TRB = 1; //重新装载计数器
Timer->RegsAddr->TCR.bit.SOFT = 0;
Timer->RegsAddr->TCR.bit.FREE = 0; // 禁止Free Run
Timer->RegsAddr->TCR.bit.TIE = 1; // 定时器中断允许
Timer->InterruptCount = 0; //复位中断计数
}