This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812CAN模块CANTA不能置位问题

最近在搞CAN通信部分,在测试TI给的例程TXLOOP.c的时候,发现程序总是停在 while(ECanaRegs.CANTA.bit.TA5 == 0 ) {} // Wait for TA5 bit to be set..这一句上,也就是说CANTA5就没有置位,然后就发送不出任何东西。查找了很多资料说是CAN总线上没有接收节点,但是在输出端TX引脚上接上示波器,没有效果;在经过CAN收发器之后,在CANH和CANL端也没有任何反应。为了测试手不是硬件问题,我用28335的开发板和demo例程也试过了,一样的问题,都是停在等待置位的那句话上。想问一下,例程里面是有BUG么?还是我需要如何外加配置才能通过?