This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP28335 XINTF硬件连接的问题



您好:

    28335的XINTF模块来外扩两片RAM,RAM1是16b*8bit,RAM2是4k*16bit。XINTF读写操作线nXRD、nXWE0和外设请求释放总线nXHOLD分别接两片RAM连接(复用),片选nXZCS0和nXZCS6分别与两片RAM连接。

问题1:地址线A0-A3、数据线D0-D7接RAM1,A0-A11和D0-D15接RAM2,(A0-A3和D0-D7复用),这样的接法是否正确?

问题2:能否地址线A0-A3、数据线D0-D7接RAM1,A4-A15和D8-D23接RAM2?这和问题1中的接法有什么区别?

问题3:对外设请求释放总线nXHOLD不是很理解,这个管脚是不是和DMA有关?是不是可以不接?

谢谢指导!