This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于F28335的两种模式的问题



在F28335的ADC模块说明PDF中,有以下2个示例:

Simultaneous Sampling Dual Sequencer Mode Example

Simultaneous Sampling Cascaded Sequencer Mode Example

有如下疑问,想请教一下:

       同步模式下,是2个采样保持器的同步(SH-A/SHB),比如ADCINA0和ADCINB0同步,级联模式下的同步,也应该是SH-A/SH-B的同步 吧?   

那上述2个示例工作状态又有什么区别呢?

  • 同步模式和级联模式,主要说是ADC的两个排序器SEQ1和SEQ2,在同步模式下独立分别控制8个转换通道,可实现ADCINAx和ADCINBx的两个通道同步转换。而在级联模式下只有SEQ1其作用,控制16个转换通道依次进行转换,这时候没有同步这一说。

  • Example 1-2. Simultaneous Sampling Cascaded Sequencer Mode Example

    这是那个示例的名称,Analog-to-Digital Converter (ADC)     21页

    级联+同步模式

  • Zone New,

    是我表述得不对。

    寄存器ADCTRL1的SEQ_CASC位是选择Dual-sequencer mode还是Cascaded mode,也就是双排序器模式还是单排序器模式,两者的区别是在触发源上可以有不同的选择;

    寄存器ADCTRL3的SMODE_SEL位选择Sequential sampling mode还是Simultaneous sampling mode,也就是顺序采样模式和同步采样模式,它们的区别是顺序采样是一个一个通道采样,同步采样是一对通道同时采样;

    上述两两组合可以形成四种模式,如Example 1-2的同步采样单排序器模式;

    另外,ADCTRL1的CONT_RUN位选择Start-stop mode还是Continuous conversion mode,即启停模式和连续采样模式,两者的区别是ADC采样频率计算方式不一样,在连续采样模式下,它的采样频率是ADCCLK/(ACQ_PS +1);在启动停止模式下,它的采样频率是SOC信号的频率。

     

  • Joey Mao

                     您解释的非常清晰明白,已了解其意思。