This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问这是什么情况?
没有什么大的区别,一个进入codestart然后进入_c_int00 ,一个是直接进入_c_int00 。
不过,我建议你还是设回到code_start,这个warning没有关系。
DSP2833x_CodeStartBranch.asm,上面有说明:
;// The compiler may warn that the entry point for the project is other then
;// _c_init00. _c_init00 is the C environment setup and is run before
;// main() is entered. The code_start code will re-direct the execution
;// to _c_init00 and thus there is no worry and this warning can be ignored.
新问题开个新帖子吧,便于其他人查询。
MOVW DP,#VAR
MOV @VAR,#0X01
和
MOVL XAR0,#VAR
MOV *XAR0,#0X01
达到的结果没有区别,只是寻址方式不同。具体您可以做个试验试一下。
详细信息可以参考:
编译出现240处“remark: zero used for undefined preprocessing identifier”,请问是怎么解决的呢?能具体说说吗?lib.谢谢了