我使用28069,采用内部时钟,之前一直使用正常,可以正常烧写和仿真,突然在一次烧写之后(一直无法擦除Flash,最后自己终止),仿真器无法连接目标板,提示如下错误信息
Error connecting to the target:
(Error -1015 @ 0x0)
Device is not responding to the request. Device may be locked, or the emulator connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 5.1.232.0)
用示波器测量XRS管脚,发现此管脚出现周期性的复位信号。
请问:这是芯片损坏了吗?或者是芯片被锁死了吗?