This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DSP与CCS5.4连接的问题

您好~

我有一个小问题,在以前CCS3.3中,只要DSP不掉电,仿真器和DSP的连接断开,只需要重新连接,仍然可以继续观察DSP内部RAM中的数据,

而在CCS5.4中,我们该如何操作完成这个目的,在CCS5.4中,我一旦DEBUG,就直接擦除RAM了.

我现在是因为程序烧在FLASH中,我想观察存在RAM中的数据,该如何操作?我不能再RAM中运行,是因为功率大了以后,DSP会与仿真器断开连接。

恳请您的帮助!

  • 只要是上电状态,用CCS重连并不会擦除掉RAM中的值呀。

    Eric

  • 在快捷操作图标栏中,debug的右边有connect / disconnect Target 图标,烧写完程序后,可以断开仿真器,只要DSP不掉电,重新连上仿真器仍然可以观察RAM中的数据,和3.3一样的