This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035 多个中断 问题



测试程序的功能如下:
Timer 1 中断定时1毫秒,Timer 2 中断定时1秒, epwm3增减计数模式,周期1毫秒,中点时触发ad采样,8个通道顺序采样1次,转换后触发ad中断,在ad中断处理程序(中断频率:1KHz)中, 通过SPI串行输出给外部DA芯片,使得输出模拟信号等于输入模拟信号。发生的问题是,
每1分钟,DA输出会被拉低几个周期,然后恢复正常,不知原因是什么?
查看了DSP2803x_SWPrioritizedIsrLevels.h, 中断优先级AD〉Timer1〉Timer2
求解