This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2406仿真复位与PDPINTB引起的复位有什么不同



2406仿真复位与PDPINTB引起的复位有什么不同

  • 我看了一下datasheet,PDPINTB是用于关断芯片的PWM的引脚,并不会引起复位,是不是有什么地方我没有理解。

    PDPINTB:

    Power drive protection interrupt input. This interrupt, when activated, puts the PWM output pins (EVB) in the

    high-impedance state should motor drive/power converter abnormalities, such as overvoltage or overcurrent, etc.,

    arise. PDPINTB is a falling-edge-sensitive interrupt.

    此外2406A已经淘汰,如果是新的研发或学习建议考虑

    www.ti.com/.../tms320f28031

  • 仿真复位是人为地手动进行软复位,PDPINT是外部信号有效时经过EV的异常处理进入中断同时产生的硬复位。

    不知道这是不是你想了解的?