This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

怎么分辨TI套件TMDSHVMTRPFCKIT属于1.7、v2.0、v2.1中的哪个版本?



怎么分辨TI套件TMDSHVMTRPFCKIT属于1.7、v2.0、v2.1中的哪个版本

  • 你好。

    1.7的板子是绿色的。

    2.0和2.1的板子都是黄色的,Controlsuit里面的软件包有更新,参见文件夹内的说明如下:

    The default project settings in HVMotorCtrl+PfcKit_v2.1 are configured for HVDMC R1.1 version (This is the kit with the yellow PCB!).
    Please refer to HVMotorCtrl+PfcKit_v1.7 or below for HVDMC R5 version.

    Changes from v2.0:
    - HVPM_sensorless project is replaced with HVPM_Enhanced_Sensorless project for 2803x devices.

  • 非常感谢,2.0和2.1硬件没差别是吧。