Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
老师您好,我最近在做28388D核间通信,现在实现的功能是将一组数据通过IPC从CPU1发送至CPU2,CPU2再使用SCIB将这组数据发送出去,但目前数据在通过SCIB发送的时候出现了问题,不能发送成功,现在将CPU1和CPU2中的代码贴出,希望老师可以帮忙寻找一下问题,非常感谢
CPU1中的代码
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Defines
//
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
#pragma DATA_SECTION(readData, "MSGRAM_CPU1_TO_CPU2")
char sdData[10]={1,2,3,4,5,6,7,8,9,'\n'};
uint32_t readData[10]={0};
uint32_t pass;
//
// Main
//
void main(void)
{
int i;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Boot CPU2 core
//
#ifdef _FLASH
Device_bootCPU2(BOOTMODE_BOOT_TO_FLASH_SECTOR0);
#else
Device_bootCPU2(BOOTMODE_BOOT_TO_M0RAM);
#endif
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
//set SCIB TX
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDB);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDB, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDB, GPIO_PIN_TYPE_STD | GPIO_PIN_TYPE_PULLUP);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDB, GPIO_QUAL_ASYNC);
GPIO_setMasterCore(DEVICE_GPIO_PIN_SCITXDB, GPIO_CORE_CPU2);
GPIO_setMasterCore(DEVICE_GPIO_CFG_SCITXDB, GPIO_CORE_CPU2);
//
// Clear any IPC flags if set already
//
IPC_clearFlagLtoR(IPC_CPU1_L_CPU2_R, IPC_FLAG_ALL);
//
// Synchronize both the cores.
//
IPC_sync(IPC_CPU1_L_CPU2_R, IPC_FLAG31);
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
//
// Fill in the data to be sent
//
for(i=0; i<10; i++)
{
readData[i] = sdData[i];
}
//
// Send a message without message queue
// Length of the data to be read is passed as data.
//
IPC_sendCommand(IPC_CPU1_L_CPU2_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
IPC_CMD_READ_MEM, (uint32_t)readData, 10);
//
// Wait for acknowledgment
//
IPC_waitForAck(IPC_CPU1_L_CPU2_R, IPC_FLAG0);
//
// Read response
//
if(IPC_getResponse(IPC_CPU1_L_CPU2_R) == TEST_PASS)
{
pass = 1;
}
else
{
pass = 0;
}
//
// End of example. Loop forever
//
while(1);
}
//
// End of File
//
CPU2中代码
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Defines
//
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
//
//Define variables
//
uint32_t recbuf[10]={0};
char recbuf1[10]={0};
//
// Function prototypes
//
__interrupt void IPC_ISR0();
//
// Main
//
void main(void)
{
int t=0;
//
// Initialize device clock and peripherals
//
Device_init();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Clear any IPC flags if set already
//
IPC_clearFlagLtoR(IPC_CPU2_L_CPU1_R, IPC_FLAG_ALL);
//
// Enable IPC interrupts
//
IPC_registerInterrupt(IPC_CPU2_L_CPU1_R, IPC_INT0, IPC_ISR0);
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//
EINT;
ERTM;
//
// Synchronize both the cores.
//
IPC_sync(IPC_CPU2_L_CPU1_R, IPC_FLAG31);
//
//Set SCIB
//
SCI_setConfig(SCIB_BASE, DEVICE_LSPCLK_FREQ, 256000, (SCI_CONFIG_WLEN_8 | SCI_CONFIG_STOP_ONE | SCI_CONFIG_PAR_NONE));
SCI_resetChannels(SCIB_BASE);
SCI_enableModule(SCIB_BASE);
SCI_performSoftwareReset(SCIB_BASE);
//
// Loop forever. Wait for IPC interrupt
//
while(1)
{
for(t=0;t<10;t++)
{
recbuf1[t]=recbuf[t];
}
for(t=0;t<10;t++)
{
if(recbuf1[t] == 0)
{
continue;
}
SCI_writeCharBlockingNonFIFO(SCIB_BASE, recbuf1[t]);
if(recbuf1[t] == '\n')
{
recbuf1[t] = 0;
break;
}
recbuf1[t] = 0;
}
}
}
//
// IPC ISR for Flag 0.
// C28x core sends data without message queue using Flag 0
//
__interrupt void IPC_ISR0()
{
int i;
uint32_t command, addr, data;
bool status = false;
//
// Read the command
//
IPC_readCommand(IPC_CPU2_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
&command, &addr, &data);
if(command == IPC_CMD_READ_MEM)
{
status = true;
//
// Read and compare data
//
for(i=0; i<data; i++)
{
recbuf[i]=*((uint32_t *)addr + i);
//if(*((uint32_t *)addr + i) != i)
//status = false;
}
}
//
// Send response to C28x core
//
if(status)
{
IPC_sendResponse(IPC_CPU2_L_CPU1_R, TEST_PASS);
}
else
{
IPC_sendResponse(IPC_CPU2_L_CPU1_R, TEST_FAIL);
}
//
// Acknowledge the flag
//
IPC_ackFlagRtoL(IPC_CPU2_L_CPU1_R, IPC_FLAG0);
//
// Acknowledge the PIE interrupt.
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}
//
// End of File
//
我在device中对如下引脚进行了定义
#define DEVICE_GPIO_PIN_SCIRXDB 11U // GPIO number for SCIB RX
#define DEVICE_GPIO_PIN_SCITXDB 10U // GPIO number for SCIB TX
#define DEVICE_GPIO_CFG_SCIRXDB GPIO_11_SCIB_RX // "pinConfig" for SCIB RX
#define DEVICE_GPIO_CFG_SCITXDB GPIO_10_SCIB_TX // "pinConfig" for SCIB TX
非常感谢老师