我编的12864液晶显示程序无法在2812开发板上显示。开发板的液晶引脚接到开发板的CPLD模块。开发板给LCD分配的地址是0x2001,我不知道程序定义了#define LCD_DATA (*((volatile Uint16 *)0x2001))这句话之后还需要定义,液晶的8 个DB口的引脚吗?需要对12864的PSB引脚的工作模式进行定义吗?我的程序没有对PSB模式进行定义,而且开发板只是给地址,并没有给出LCD引脚具体链接到哪个GPIO口,所以我也不知道如何给PSB引脚进行赋值。我觉得我的程序问题应该出在GPIO的定义,和PSB引脚上。附件中有我的源程序,其中GPIO和LCD这两个源文件是我自己编写的。新手初学,麻烦请帮我看看,谢谢啦!