专家你好
我用的MCU 是28335,电源芯片是tps767d318。有个问题特向您请教。就是tps767d318的1.8V和3.3V输出是同步的,直接接在28335有没有问题。需不需要在1.8V输出做延时处理。我记得以前2812,1.8v输出必须要有延时的,要不然,片子不工作。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
专家你好
我用的MCU 是28335,电源芯片是tps767d318。有个问题特向您请教。就是tps767d318的1.8V和3.3V输出是同步的,直接接在28335有没有问题。需不需要在1.8V输出做延时处理。我记得以前2812,1.8v输出必须要有延时的,要不然,片子不工作。谢谢!
可以不需要的,这正是F2833x相比F281x改进的很重要的一点。
在F2833x上,对上电时序没有特别的要求,当然如果1.8V不晚于3.3V是最好的,只要保证3.3V到达0.7V之前,1.8V已经过了0.7V. 具体请参考数据手册 www.ti.com/lit/SPRS439 第128页 6.8 Power Sequencing.
实际上,其下方的Table 6-10. Power Management and Supervisory Circuit Solutions也有建议一些其它的LDO和DC/DC给F2823x/33x供电。