This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

提高F28335采样率问题



F28335技术手册上面说,内部ADC最高采样率顺序采样可达到8M左右,同步采样可以达到4M左右,我采用的PWM触发其ADC同步采样,只读取一个通道的值,最高采样率可以达到750K,却提高不上去了,ADC时钟设置最高和采样保持时间设置最短,请问F28335技术手册上面说的那么高的采样率怎么达到哈?或者F28335技术手册上面的几M采样率是几个通道合起来的采样率?请各位大神帮忙解决,谢谢!

  • 手册上说的采样率是不是用其他触发方式触发的     你得到的750K是指的触发ADC的PWM频率吗

     

  • 手册上也没有具体说明采样率是不是用其他触发方式触发的 ,不知道您可不可以提高采样率呢? 我得到的750K是指的触发ADC的PWM频率,同时也是ADC进中断和出中断的频率,我是通过拉高拉低一个IO口来观察ADC的采样率的;当我提高触发ADC的PWM频率大于750K时,发现不能有效触发ADC去采样,意思是触发频率太高有的触发信号是无效的。如果不用PWM触发,那么还有什么好的办法来提高采样率呢,有改过的例程那就最好啦,我试过很多次都没成功,希望您能帮我解决,谢谢!

  • 手册标识的采样频率是指ADC采样保持器的速度,你用的测试方法其中会涉及转换时间已经进出中断时间都会有CPU Clock的delay。所以并不是准确的数据。

  • 怪不得我实测的AD采样率和手册上差别那么多,根本达不到手册上的采样率,也和算出来的理想采样率不一致

    搞得我一切都以实测值为准

  • 你好,我还是想问一下您,那我该如何更好地测试我的ADC真实的采样速率呢?我只是保证了基本的取ADC寄存器的值得几段语句再加上IO口拉高拉低的语句,这几句我看了一下系统运行时间,远小于1/750K的时间哈,您的意思还有出中断和进中断的时间,那也很小哈,是不是触发ADC的方式不对?还有,我想问一下您,您在实际中能够达到的最高采样率到多少呢?谢谢您的回答!

  • AD实测采样率我最高是3M不到。

    最简单的方法:一般的示波器都有一个基准方波信号,1KHZ(周期1ms),你让28335采这个信号,CCS里用数组存下来,导入EXCEL,画个图(插入->折线图),看1个周期有多少个数据,再除以1ms,就是采样率。如图

    SAMPLE RATE = 168 SAMPLS/ 1ms = 168 000 Samples/s = 168K.

  • 你好,试了您的方法,可以看出采样率。但是我的最高采样率还是750kHz,我采用的是PWM触发采样的,同步采样模式,在ADC中断中将数据存入数组。能不能把您的ADC采样率3M的那个ADC初始化程序发给我学习一下不?真的纠结了好久啦,谢谢您。

  • 我这里是采4个通道,每个通道 600多K,和你的采用PWM方式不一样,我采用的方法是用一个脉冲产生AD转换,然后AD自动转换,DMA送到内存。

    /***************************************************************************
    If the cascaded SEQ was executed, the results would go to the following ADCRESULT registers:
    ADCINA0 -> ADCRESULT0
    ADCINB0 -> ADCRESULT1
    ADCINA1 -> ADCRESULT2
    ADCINB1 -> ADCRESULT3
    ADCINA2 -> ADCRESULT4
    ADCINB2 -> ADCRESULT5
    ADCINA3 -> ADCRESULT6
    ADCINB3 -> ADCRESULT7
    ADCINA4 -> ADCRESULT8
    ADCINB4 -> ADCRESULT9
    ADCINA5 -> ADCRESULT10
    ADCINB5 -> ADCRESULT11
    ADCINA6 -> ADCRESULT12
    ADCINB6 -> ADCRESULT13
    ADCINA7 -> ADCRESULT14
    ADCINB7 -> ADCRESULT15
    ****************************************************************************/
    void ADCConfig(void)
    {
        //InitAdc();
        //AdcRegs.ADCREFSEL.bit.REF_SEL = 0x0;   // 00,Internal reference selected (default)
        //AdcRegs.ADCTRL1.bit.ACQ_PS = 0xF;       // This bit field controls the width of SOC pulse,
        //AdcRegs.ADCTRL1.bit.CONT_RUN = 0;       // 0/1:Start-stop mode/Continuous conversion mode
        //AdcRegs.ADCTRL1.bit.SEQ_OVRD = 0;       // Sequencer override Disabled,Allows the sequencer to wrap around at the end of conversions set by MAX_CONVn
        //AdcRegs.ADCTRL1.bit.SEQ_CASC = 1;       // Cascaded mode. SEQ1 and SEQ2 operate as a single 16-state sequencer (SEQ).
        //AdcRegs.ADCTRL1.bit.CPS = 0;           // 0:ADCCLK = Fclk/1; 1:ADCCLK = Fclk/2; Fclk = Prescaled HISPCLK;   NOTE:  HISPCLK = SYSCLKOUT/2,

        //AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;    // Setting this bit allows the cascaded sequencer to be started by an ePWM SOCB signal
        //AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;           // Immediately reset sequencer to state CONV00
        //AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;   // Interrupt request by INT_SEQ1 is enabled.
        //AdcRegs.ADCTRL3.bit.ADCCLKPS = 0x3;        // Core clock divider,  HISPCLK = SYSCLKOUT/2, 75M/6 = 12.5Mhz, 12.5M/(0+1) = 12.5Mhz,
        //AdcRegs.ADCTRL3.bit.SMODE_SEL = 1;        // 0/1,Sequential/Simultaneous sampling mode is selected
        //AdcRegs.ADCMAXCONV.all = 0;    //AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0;    // ADC Input Channel Selected


        InitAdc();
        AdcRegs.ADCTRL3.bit.SMODE_SEL = 1;       // 0/1,Sequential/Simultaneous sampling mode is selected
        AdcRegs.ADCTRL1.bit.SEQ_CASC = 1;        // 0/1,separate mode/ Cascaded mode. SEQ1 and SEQ2 operate as a single 16-state sequencer (SEQ).
        AdcRegs.ADCMAXCONV.all = 0x07;           // 8 double conv's (4 total),The sequence naturally wraps around at the end of the MAX_CONVn setting.

        AdcRegs.ADCREFSEL.bit.REF_SEL = 0x0;     // 00,Internal reference selected (default)
        AdcRegs.ADCTRL1.bit.ACQ_PS = 0x1;        // This bit field controls the width of SOC pulse,0x0F
        AdcRegs.ADCTRL1.bit.CONT_RUN = 1;        // 0/1:Start-stop mode/Continuous conversion mode
        AdcRegs.ADCTRL1.bit.SEQ_OVRD = 0;        // Sequencer override Disabled,Allows the sequencer to wrap around at the end of conversions set by MAX_CONVn

        AdcRegs.ADCTRL1.bit.CPS = 0;             // 0:ADCCLK = Fclk/1; 1:ADCCLK = Fclk/2; Fclk = Prescaled HISPCLK;   NOTE:  HISPCLK = SYSCLKOUT/2,

        //AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 0;  // Setting this bit allows the cascaded sequencer to be started by an ePWM SOCA signal
        AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1;          // Immediately reset sequencer to state CONV00
        AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1;      // Interrupt request by INT_SEQ1 is enabled to trigger DMA transfer, no need to implement SEQ1 ISA
        AdcRegs.ADCTRL3.bit.ADCCLKPS = 0x2;        // Core clock divider,  HISPCLK = SYSCLKOUT/2, 75M/6 = 12.5Mhz, 12.5M/(0+1) = 12.5Mhz

        // ACQ_PS = 0x01, ADCCLKPS = 0x0   can not convert analog correctly
        // ACQ_PS = 0x01, ADCCLKPS = 0x1   615k samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x2   590K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x3   390K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x4   290K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x5   232K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x6   194K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x7   164K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x8   143K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0x9   130K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0xA   114K samples /second
        // ACQ_PS = 0x01, ADCCLKPS = 0xB   104K samples /second

        // ACQ_PS = 0xF, ADCCLKPS = 0x3      15K samples /second

        AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0;     // ADC Input Channel Selected,ADCINA0/ADCINB0
        AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1;     // ADC Input Channel Selected,ADCINA1/ADCINB1
        AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x0;     // ADC Input Channel Selected,ADCINA0/ADCINB0
        AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x1;     // ADC Input Channel Selected,ADCINA1/ADCINB1
        AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x0;     // ADC Input Channel Selected,ADCINA0/ADCINB0
        AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x1;     // ADC Input Channel Selected,ADCINA1/ADCINB1
        AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x0;     // ADC Input Channel Selected,ADCINA0/ADCINB0
        AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 0x1;     // ADC Input Channel Selected,ADCINA1/ADCINB1
     
    }

    希望对你有帮助

  • 您好,很高兴收到您的回复,我有时间来验证一下哈。还有我想问一下您,您是不是拿600k乘以4得到2.4M的采样率哈,那如果我只采集一个通道,可不可以达到2.4M采样率呢?希望您百忙之中能回复我一下,谢谢您。

  • 你好,我也是在做28335的采样,同样是用epwm来触发adc采样的,在采样率的设置上的实现问题,想请教你一些问题,不知道能不能加好友交流,QQ:975954022