This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C28346的eCAP中断



各位开发者:

    大家好。我使用C28346的eCAP1进行外部信号的上升沿捕捉,在GPIO24管脚上有一个20MHz的时钟信号,我在eCAP1的中断函数中进行计数。参考了TI提供的eCAP的例程,发现eCAP工作在One-shot模式下,我现在把其改成了连续模式,发现中断只执行一次就停止了,寄存器的配置如下:

   ECap1Regs.ECEINT.all = 0x0000;             // Disable all capture interrupts
   ECap1Regs.ECCLR.all = 0xFFFF;              // Clear all CAP interrupt flags
   ECap1Regs.ECCTL1.bit.CAPLDEN = 0;          // Disable CAP1-CAP4 register loads
   ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0;        // Make sure the counter is stopped
  
   // Configure peripheral registers
   ECap1Regs.ECCTL2.bit.CONT_ONESHT = 0;      //
   ECap1Regs.ECCTL2.bit.STOP_WRAP = 3;        // Stop at 4 events
   ECap1Regs.ECCTL1.bit.CAP1POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP2POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP3POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CAP4POL = 0;          // Rising edge
   ECap1Regs.ECCTL1.bit.CTRRST1 = 0;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST2 = 0;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST3 = 0;          // Difference operation
   ECap1Regs.ECCTL1.bit.CTRRST4 = 0;          // Difference operation
   ECap1Regs.ECCTL2.bit.SYNCI_EN = 0;         // Enable sync in
   ECap1Regs.ECCTL2.bit.SYNCO_SEL = 0;        // Pass through
   // ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable capture units


   ECap1Regs.ECCTL2.bit.TSCTRSTOP = 1;        // Start Counter
   ECap1Regs.ECCTL1.bit.CAPLDEN = 1;          // Enable CAP1-CAP4 register loads
   ECap1Regs.ECEINT.bit.CEVT4 = 1;            // 4 events = interrupt

请教下原因是什么?该如何才能让eCAP工作在连续模式下进行中断?