This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2812的.cinit段只能放在FLASHA和FLASHB?



我的项目中,FLASHA已经被bootloader占用,用户程序只能放到FLASHA以外的FLASH,实际中发现.cinit段放到FLASHC以后的段,代码运行异常,放到FLASHB可以运行,请TI的工程师帮忙验证一下问题,谢谢。

  • .cinit用于放置初始化的变量和常量表,没有规定只能放到FlashA和FlashB,但要求放在程序页

  • FLASH C在CMD文件中是放在PAGE0中的吗?

  • 是在PAGE0的,事实上,我所有FLASH都放到PAGE0了。
    跟踪代码发现 在RTS库的boot28.inc文件中初始化cinit部分的代码跑飞了。因为.cinit段放到FLASHB功能正常,没有深究这段代码。

    MOVL XAR7,#cinit ; point XAR7 at start of table
    CLRC TC ; reset TC bit used as far flag 

    B START, UNC ; jump to start processing
    LOOP:
    MOVB AH,#0 ; zero out upper addr bits
    PREAD AL,*XAR7 ; load address of variable to be inited
    ADDB XAR7,#1 ; point to initialization data
    B GET_DATA,NTC ; get data if variable is not far
    CLRC TC ; reset TC bit used as far flag
    PREAD AH,*XAR7 ; otherwise, get hi bits of 22-bit addr
    ADDB XAR7,#1
    GET_DATA:
    MOVL XAR6,ACC ; address
    RPT AR1 ; repeat length + 1 times
    || PREAD *XAR6++,*XAR7 ; copy data from table to memory

    MOVL ACC,XAR7 ; using ACC as temp, point XAR7 to
    ADD ACC,AR1 ; next cinit record since PREAD
    ADDB ACC,#1 ; doesn't change value of XAR7.
    MOVL XAR7,ACC
    START:
    PREAD AL,*XAR7 ; load length
    B GET_ADDR,GEQ ; a length < 0 denotes far data
    NEG AL ; negate value to get real length
    SETC TC ; flag that the address field is 32-bits
    GET_ADDR:
    MOVZ AR1,AL ; copy length value to loop register
    ADDB XAR7,#1 ; point to address field
    BANZ LOOP,AR1-- ; if (length-- != 0) continue

     

  • 楼主,请问你的bootloader是如何定义到FLASHA上的?我最近也在写bootloader,不想用片子内置的,CMD要如何配置,求高人解答,谢谢!