This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: DAC输出问题

Part Number: TMS320F28377D

请问手册中写的DAC的输出是0.3-VDDA,其中VDDA是3.3V直流加上100mv交流,那么是不是代表DAC的输出可能存在mv级别的交流耦合在直流上?

  • 手册里面的上电时间最长是500us,我根据device_support中的示例设置为20us,DAC输出经过跟随电路,跟随电路的输出一直耦合有一个峰值为50mv,频率为50kHz的锯齿波,当我把上电延时时间设置为500us时,这个锯齿波变为峰值为20mv,频率为50kHz的锯齿波,两种上电时间下DAC的输出即跟随电路的输入都没有干扰信号,请问这是什么原因?

  • 跟随电路用的运放是op367