This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C28346的XINTF应用



在使用C28346与FPGA进行XINTF操作时遇到了一些问题:

1)C28346在使用XINTF时,地址总线是否需要释放?如果释放,何时、如何释放?

2)C28346的XINTF进行读操作和写操作时,是否需要释放数据总线?如果需要释放,何时、如何释放?是否需要上拉?

3)C28346在使用XINTF的XREADY功能时,是否是在ACTIVE阶段才对XREADY管脚进行采样?在LEAD或者TRAIL阶段出现XREADY信号是否会产生影响?

  • 你好!最近我也在调试28346与FPGA的XINTF操作。在16位数据总线模式下,DSP既能够读FPGA发送来的数据也能够发送数据给FPGA,但是在32位数据总线模式下,DSP只能发送数据给FPGA,不能收到FPGA发送来的数据,您觉得可能是什么问题?麻烦您指导一下,谢谢!