This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV6编译TI例程出错



你好,我使用TI 281x的例程在CCSV6的开发环境下进行编译,编译结果总是如下:

>> Compilation failure
'Building file: E:/TI/281x/v120/DSP281x_common/source/DSP281x_PieVect.c'
'Invoking: C2000 Compiler'
"c:/ti/ccsv6/tools/compiler/c2000_6.2.5/bin/cl2000" -v28 -ml -mt --include_path="c:/ti/ccsv6/tools/compiler/c2000_6.2.5/include" --include_path="E:/TI/281x/v120/DSP281x_headers/include" --include_path="E:/TI/281x/v120/DSP281x_common/include" -g --define="_DEBUG" --define="LARGE_MODEL" --quiet --diag_warning=225 --issue_remarks --asm_directory="C:/tidcs/c28/DSP281x/v120/DSP281x_examples_ccsv4/adc_seqmode_test/Debug" --preproc_with_compile --preproc_dependency="DSP281x_PieVect.pp"  "E:/TI/281x/v120/DSP281x_common/source/DSP281x_PieVect.c"
Command-line error: cannot open command file '\\DOCUME~1\\ADMINI~1\\Temp\\0579214': No such file or directory
1 catastrophic error detected in this compilation.
Compilation terminated.

>> Compilation failure
gmake: *** [DSP281x_PieVect.obj] Error 1

工程中的每一个源文件都报如上所示的错误,请问这是什么原因?