This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28027电源脚的问题



我想做一个28027的最小系统板。
有两个问题:
1.第11脚VDDA.我们公司原来做了一个28335的板子,我看电源有3.3V和1.9V
那28027电源脚是不是都是接3.3V?我吃不准。请高手指教,谢谢!
2.Single Supply Source when VREG is enabled
我觉得意思是当VREG(内部电压调节器)使能时,单电源供电。
那是不是说,当使能VREG时,这个脚上自动输出一个电源电压,不需要外部
再接电源了,是吗?请指教,谢谢!