This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PWM输出有异常情况发生



DSP 的PWM在使用的时候,通过程序不断的更新寄存器的CMPA/CMPB映射单元的值,并在特定的情况下将映射寄存器的值装载到当前寄存器。

但是在某些情况下,新的输出比较值会滞后一个PWM周期输出,而前一次的寄存器比较值会延时一个周期。

有谁知道这里的某些情况是什么情况,有什么可以防止的方法? 

  • 请具体描述你的问题,比如如何配置PWM,产生问题的图是怎么样的?

  • 整个程序的思想是AD 实时采样,用PWM实时输出AD的采样值,把PWM当DA用。

    PWM的配置如下:

    EPwm1Regs.TBPRD =CC_TBPRD; 
    EPwm1Regs.TBCTL.all = 0;   
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV2; 
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; 
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; 

    EPwm1Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW ;
    EPwm1Regs.CMPCTL.bit.LOADAMODE=CC_CTR_PRD;

    EPwm1Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm1Regs.AQCTLA.bit.PRD=AQ_CLEAR;

    EPwm1Regs.CMPA.half.CMPA=0;

    下面是AD中断的程序,意思是在每个AD采样中断中修改一次PWM的CMPA的值。CMPA与AD采样值有一个对应的关系,使得PWM的占空比与AD采样值成正比关系。AD采样率与PWM同频。AD配置以及中断配置这里没有写,可以正常工作。

    interrupt void adc1_isr(void)
    {
    AD_result_A0= Adc1Result.ADCRESULT0;

    Value_CMPA1=CC_TBPRD-AD_result_A0*Value_num;

    EPwm1Regs.CMPA.half.CMPA=Value_CMPA1;

    Adc1Regs.ADCINTFLGCLR.bit.ADCINT1 = 1;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;

    }

    (为了清晰描述这个问题,不考虑AD过采样)现在AD用10K的采样速度采集5K的的输入信号,也就是输入信号一个周期有两个采样值,对应的PWM占空比应该变化两次。但是出现了下图中的问题,在某个地方,CMPA的值与理论上采样值不对应的情况。现在已证实AD采样值是没有错误的,揣测是CMPA的值有的时候没有装载到当前寄存器上或者是什么原因。

  • 5k的输入信号是什么波形,另外触发采样点在哪里?怎么设置的?

  • 输入信号时5K的正弦信号。

    用的是F28M35x开发板,下面是C28x整个的程序

    #include "DSP28x_Project.h" // Device Headerfile and Examples Include File
    #include <string.h>

    #define C28_FREQ 150 //C28 CPU frequency in MHz
    #define CC_TBPRD 7500

    extern Uint16 RamfuncsLoadStart;
    extern Uint16 RamfuncsLoadSize;
    extern Uint16 RamfuncsRunStart;

    float Value_num;

    interrupt void adc1_isr(void);
    //interrupt void Epwm1_INT_isr(void);

    Uint16 AD_result_A0;
    Uint16 Value_CMPA1;


    void main(void)
    {
    InitSysCtrl(); // Init C28 core
    EALLOW;
    GpioG1CtrlRegs.GPADIR.bit.GPIO4 = 1; // GPIO4 as output
    GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 1; // GPIO0 = ePWM1A
    EDIS;

    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);

    InitFlash();

    Value_num=CC_TBPRD/4095.0;

    DINT;
    InitPieCtrl();
    IER=0x0000;
    IFR=0x0000;
    InitPieVectTable();
    EALLOW; // This is needed to write to EALLOW protected registers
    PieVectTable.ADCINT1 = &adc1_isr;
    EDIS;


    InitCpuTimers();
    ConfigCpuTimer(&CpuTimer0, C28_FREQ, 100); //SOC
    //Enable INT
    PieCtrlRegs.PIEIER1.bit.INTx1 = 1;
    IER |= M_INT1;
    EINT; // Enable Global interrupt INTM
    ERTM; // Enable Global realtime interrupt DBGM

    //configure EPwm1
    EPwm1Regs.TBPRD =CC_TBPRD; //
    EPwm1Regs.TBCTL.all = 0; // clear all bits in TBCTL
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV2; // CLKDIV = 2
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; // HSPCLKDIV =1
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // count mode = up-mode
    //fpwm =fcpu / ( TBPRD * CLKDIV * HSPCLKDIV)

    EPwm1Regs.CMPCTL.bit.SHDWAMODE=CC_SHADOW ;
    EPwm1Regs.CMPCTL.bit.LOADAMODE=CC_CTR_PRD;

    EPwm1Regs.AQCTLA.bit.CAU=AQ_SET;
    EPwm1Regs.AQCTLA.bit.PRD=AQ_CLEAR;

    EPwm1Regs.CMPA.half.CMPA=0;


    //configure ADC 
    InitAdc1();
    EALLOW;
    Adc1Regs.ADCCTL2.bit.ADCNONOVERLAP = 1; 
    Adc1Regs.ADCCTL1.bit.INTPULSEPOS = 1; // ADCINT1 trips after AdcResults latch
    Adc1Regs.INTSEL1N2.bit.INT1E = 1; // Enabled ADCINT1
    Adc1Regs.INTSEL1N2.bit.INT1CONT = 0; // Disable ADCINT1 Continuous mode
    Adc1Regs.INTSEL1N2.bit.INT1SEL = 0; // setup EOC0 to trigger ADCINT1 to fire

    Adc1Regs.ADCSOC0CTL.bit.CHSEL = 0; // set SOC0 channel select to ADC1in_B0
    Adc1Regs.ADCSOC0CTL.bit.TRIGSEL = 5; // Set SOC0 start trigger to trigger1 // ADC Trigger 1 of the ADC
    Adc1Regs.ADCSOC0CTL.bit.ACQPS =6; // set SOC0 S/H Window to 7 ADC

    AnalogSysctrlRegs.TRIG1SEL.all = 1; // Assigning TINT0 to ADC-TRIGGER 1 // Clock Cycles, (6 ACQPS + 1)
    EDIS;

    CpuTimer0Regs.TCR.bit.TSS = 0; // start T0
    while(1)
    {

    }
    }

    interrupt void adc1_isr(void)
    {
    AD_result_A0= Adc1Result.ADCRESULT0;

    Value_CMPA1=CC_TBPRD-AD_result_A0*Value_num;

    EPwm1Regs.CMPA.half.CMPA=Value_CMPA1;

    Adc1Regs.ADCINTFLGCLR.bit.ADCINT1 = 1;
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;

    GpioG1DataRegs.GPADAT.bit.GPIO4 ^= 1;
    }

    放了一个GPIO04 的电平反转在AD中断中看AD采样的频率是否正常,可以看到频率是5K,脉宽有5ns到50ns的变化。  

  • 最后的原因是 PWM分频后的TBCLK与 AD 的trigger Timer0 有频差