This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

带CLA加速器的程序有RAM导入到FLASH中运行的问题



之前调试通过的带CLA加速器的程序导入FLASH中,并采用FLASH_CLA_C.CMD配置文件,编译的时候发现有警告:

Description Resource Path Location Type #10247-D creating output section "ADCDRV_1ch_CLA_Section" without a SECTIONS

Description Resource Path Location Type #10247-D creating output section "CNTL_2P2Z_CLA_Section" without a SECTIONS

等类似的情况,由于是警告,所以我想问,这些警告是否可以忽略,或者是否要在CMD文件中增加“section :  ADCDRV_1ch_Section    : > dataRAM    PAGE = 1”之类的指定代码?谢谢你的回复