使用的CCS10,用XDC100V2给28066烧录代码,仿真器可以正常连接,但是烧录时提示等待目标停止超时,请问会是什么原因呢

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.配置的是GetMode模式,但是有时候可以正常烧录,有时候烧录到一半就报出超时。请问使用CCS10进行烧录的时候,对仿真器的版本有要求吗?我用的是XDC100V2版本
2.下面是使用XDC100V3烧录报出的错误:
C28xx: Failed CPU Reset: (Error -1041 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129)
C28xx: GEL: Error calling OnPreFileLoaded(): Reset failed: retcode=-1
C28xx: Failed CPU Reset: (Error -1140 @ 0x0) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
C28xx: Error occurred during flash operation: CPU Reset error. Error code -1
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Failed CPU Reset: (Error -1138 @ 0x0) Device refused to allow debug mode. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
C28xx: Error occurred during flash operation: CPU Reset error. Error code -1
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: D:\zhuhongwei\Project\P36SH\code\P36SH_28066_V1.0.1\Master_DSP\Output\P3600SH_28066.out: Load failed.
下面故障是使用XDC100V2烧录报出的。现象是:擦除到一半,然后提示Timed out waiting for target to halt ,然后我发现此时芯片的XRS会被拉低复位一下。
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: D:\zhuhongwei\Project\P36SH\code\P36SH_28066_V1.0.1\Master_DSP\Output\P3600SH_28066.out: Load failed.
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: D:\zhuhongwei\Project\P36SH\code\P36SH_28066_V1.0.1\Master_DSP\Output\P3600SH_28066.out: Load failed.
擦除完成,开始烧录就卡主,然后报故障,经常出现这种情况,已经因为这个原因导致几块DSP锁住没法解锁了,麻烦帮忙分析一下是什么原因?
C28xx: Flash Programmer: Error encountered when writing to flash memory C28xx: File Loader: Memory write failed: Unknown error C28xx: GEL: File: D:\zhuhongwei\Project\P36SH\code\BootLoader_28066\SCI_test\Debug\Bootloader_DSP1.out: Load failed. C28xx: Error: (Error -1135 @ 0x8999) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129) C28xx: Unable to determine target status after 20 attempts C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging C28xx: Error connecting to the target: (Error -1135 @ 0x8999) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129) C28xx: Error connecting to the target: (Error -1135 @ 0x8999) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.4.0.00129) C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface2806xV1_00.out C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled. C28xx: File Loader: Memory write failed: Unknown error C28xx: GEL: File: D:\zhuhongwei\Project\P36SH\code\BootLoader_28066\SCI_test\Debug\Bootloader_DSP1.out: Load failed.
参考下手册中下面这段:

你的板子应该是锁死了,是无法解锁的。
鉴于我都是在擦除完成烧录开始就出现烧录中断
建议你先用TI的例程试一下,看是否为你的程序问题。
我不使用FlashA区(我把代码放到flashB~H区),是不是可以避免DSP由于烧录出现中断导致DSP锁死?
你可以尝试一下。