This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
编译不通过,出现
Error: Cannot find module 'C:\dot_file_libraries\clbDotUtility.js' at Function.Module._resolveFilename (internal/modules/cjs/loader.js:880:15) at Function.Module._load (internal/modules/cjs/loader.js:725:27) at Function.executeUserEntryPoint [as runMain] (internal/modules/run_main.js:72:12) at internal/main/run_main_module.js:17:47 { code: 'MODULE_NOT_FOUND', requireStack: []
问题在于Build—Steps—Post-build steps 中多了一些代码,但我不知道他们起到什么作用。
mkdir "${BuildDirectory}/simulation" ${CLB_SIM_COMPILER}/g++ -c -DCLB_SIM -I${SYSTEMC_INSTALL}/src -I${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/include -I${PROJECT_ROOT} -I${CLB_SIM_COMPILER}/include -Og -g -gdwarf-3 -gstrict-dwarf -Wall -MMD -MP -MF${BuildDirectory}/simulation/clb_sim.d -MT${BuildDirectory}/simulation/clb_sim.o -I${BuildDirectory}/syscfg -fno-threadsafe-statics -o${BuildDirectory}/simulation/clb_sim.o ${BuildDirectory}/syscfg/clb_sim.cpp ${CLB_SIM_COMPILER}/g++ -DCLB_SIM -Og -g -gdwarf-3 -gstrict-dwarf -Wall -Wl,-Map,${BuildDirectory}/simulation/simulation_output.map -L${SYSTEMC_INSTALL}/build/src -o${BuildDirectory}/simulation/simulation_output.exe ${BuildDirectory}/simulation/clb_sim.o ${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/src/CLB_FSM_SC_model.o ${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/src/CLB_HLC_SC_model.o ${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/src/CLB_LUT4_SC_model.o ${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/src/CLB_OutputLUT_SC_model.o ${C2000WARE_ROOT}/utilities/clb_tool/clb_syscfg/systemc/src/CLB_counter_SC_model.o -Wl,--start-group -lsystemc -Wl,--end-group ./simulation/simulation_output.exe ${NODE_TOOL} "${CLB_SYSCFG_ROOT}/dot_file_libraries/clbDotUtility.js" "${CLB_SYSCFG_ROOT}" "${BuildDirectory}/syscfg" "${BuildDirectory}/syscfg/clb.dot"
你好,参考下工程师的回复:
The post-build step regarding the clbDotUtility.js is used to generate the diagram for the CLB Tool; if you're not using it you can exclude the step by setting the NODE_TOOL variable to 0 in the Project Properties Build settings.
If you are trying to generate a diagram for the CLB Tool, verify that the Linked Resources section of the Project Properties lists CLB_SYSCFG_ROOT as something like: C2000Ware_4_XX_XX_XX\utilities\clb_tool\clb_syscfg\dot_file_libraries, because otherwise it will always have this error.