This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: 中断的响应速度

Part Number: TMS320F280049C
Other Parts Discussed in Thread: LAUNCHXL-F280049C

采用EPWM中断,在TB为0进行响应,在中断中翻转设定的一个GPIO电平,发现进入中断以及拉高电平这个过程中花费了330ns,这个时间对应200kHz的控制有些太长,该现象是否正常是否有改进空间

Using EPWM interrupt and responding to the TB is zero, flipping a set GPIO level during the interrupt found that it took 330ns to enter the interrupt and raise the level. This time corresponds to a somewhat long control time of 200kHz. Is there room for improvement in this phenomenon

  • 你好,你使用的是什么板子?是自己做的板子吗?

    请参考下数据表中对中断时序的描述:

    GPIO电平翻转时间负载为40pf时为8ns。

  • 采用的是LAUNCHXL-F280049C电路板,其设定其在PWM TB模块中 CTR等于0时触发中断,并且进入中断时立即翻转GPIO,同时PWM设定在CTR等于0时刻EPWM输出IO电平置0,分析了该下降沿以及翻转IO口电平的时间差为330ns,请问这个时间有可能是进入中断并翻转的时间吗?GPIO时间8ns的话,中断响应过程为何如此之长

  • 请参考下下图,

    请问这个时间有可能是进入中断并翻转的时间吗?

    应该是中断延时时间+GPIO翻转时间。