This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs4.2.5编译问题



工程文件经过编译后如下问题:

undefined first referenced            

 symbol       in file                

--------- ----------------            

U$$MOD    ./Example_2806xAdcSoc.obj  

_c_int00  ./F2806x_CodeStartBranch.obj

error: unresolved symbols remain

warning: entry-point symbol other than "_c_int00" specified:  "code_start"

error: errors encountered during linking; "Example_2806xAdcSoc.out" not built

>> Compilation failure

gmake: *** [Example_2806xAdcSoc.out] Error 1

gmake: Target `all' not remade because of errors.

Build complete for project ORIGINAL_PROJECT_ROOT

Errors提示如下:

Severity and Description Path Resource Location Creation Time Id

errors encountered during linking; "Example_2806xAdcSoc.out" not built ORIGINAL_PROJECT_ROOT line 0 1334020979640 207

unresolved symbol _c_int00, first referenced in ./F2806x_CodeStartBranch.obj ORIGINAL_PROJECT_ROOT line 0 1334020979640 205

unresolved symbol U$$MOD, first referenced in ./Example_2806xAdcSoc.obj ORIGINAL_PROJECT_ROOT line 0 1334020979640 204

请问是什么原因? 是否是因为编译环境设置有问题? 有没有相关编译环境配置的相关资料?

  • 这个报错,我估计是没有正确引用库文件的报错,除了上次谈到的环境变量设置,也请确认一下有正确包含TI的库文件。就我所知没有专门讨论环境变量的资料,你可以在CCS-->help中查询一下,会有一些零散的地方偶尔提及这方面的内容。