第一次设计2808的板子,发现2808在跑程序的时候发热很厉害,没跑程序的时候整个板子的电流不到0.1A(12V),跑其程序来先是在0.15A(12V)停留几秒,然后又快速的升到0.28A(12V),想问的是这是跑程序时正常的过程吗?电源设计使用了一个DCDC从12V降压到5.4。然后分出5V,3.3V和1.8V。
对了,这个板子的面积有些小,只有4.5×4厘米,电源芯片的热量会影响到DSP的工作电流吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
第一次设计2808的板子,发现2808在跑程序的时候发热很厉害,没跑程序的时候整个板子的电流不到0.1A(12V),跑其程序来先是在0.15A(12V)停留几秒,然后又快速的升到0.28A(12V),想问的是这是跑程序时正常的过程吗?电源设计使用了一个DCDC从12V降压到5.4。然后分出5V,3.3V和1.8V。
对了,这个板子的面积有些小,只有4.5×4厘米,电源芯片的热量会影响到DSP的工作电流吗?
测了一下1.8V的电流,跑到了0.25A
内核和逻辑电源口IDD跑到0.25A稍稍超出了最大值,但是没有之前测板子的12V跑到0.28A这么夸张。板子上有什么高功耗的器件吗?结合IDD也偏大,先排查板子上有没有短路的地方。
可以结合ZHCS898O_TMS320F280x、TMS320C280x、TMS320F2801x 数字信号处理器 datasheet (Rev. O)的5.5 Power Consumption Summary来检查。Table 5-1结合这些部分来看:
- P23
- P22
- P17
- P15