This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: GPIO20功能异常,无法作为普通I/O口输出

Part Number: TMS320F280039C

为何280039C开发板配置GPIO20为普通输出口,该口输出电压为1.73V无法实现高低电平的功能?

代码如下

EALLOW;

GpioCtrlRegs.GPAPUD.bit.GPIO20 = 1; //Dispull up
GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 0;
GpioCtrlRegs.GPADIR.bit.GPIO20 = 1; //0: input 1:output.
GpioDataRegs.GPACLEAR.bit.GPIO20 = 1; //高电平有效,默认低电平

EDIS;

GpioDataRegs.GPATOGGLE.bit.GPIO20 = 1;//for debug