This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS470R1B1M MCU program cannot be downloaded

Part Number: TMS470R1B1M

Question:

(1)TMS470R1B1M  microcontroller is stuck in the Busy interface during the program debugging, and the program cannot be downloaded. At present, two single-chip computers have the same problem. At first, the single-chip computer program can be downloaded, after a period of use, the program can't be downloaded.

Phenomenon:

the working voltage and current of the circuit board are normal, the output signal of the crystal oscillator is normal, and the two reset pins are normal, but the program cannot be downloaded.

(2)With SEGGER J-Flash connection, prompt:

Could not detect CPU clock speed.Readback of test code download into RAM failed.

Failed to measure CPU clock frequency

Failed to connect