This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386S: How to execute the classic CAN through MCAN module in the Cortex -A4?

Part Number: TMS320F28386S


I want to use the classic CAN communication in the cortex-A4.

First I set the parameters in CPU1.

    // Allocate MCAN (a shared peripheral) to cortex-A4 (C28x)
    SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_MCAN_A,0x1U);

    // Configure the divisor for the MCAN bit-clock
    SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_4);

    // Configuring the GPIOs for MCAN.
    GPIO_setPinConfig(GPIO_10_MCAN_RX);
    GPIO_setPinConfig(GPIO_4_MCAN_TX);

Then, I configure the parameters in Cortex-A4.

    // Switching on the peripheral.
    CM_init();

    // Reset the peripheral.
    SysCtl_resetPeripheral(SYSCTL_PERIPH_RES_MCAN_A);

    // CrossBar and ISR Configuration.
    MCANIntrConfig();

    //
    // Configure the MCAN Module.

    MCANConfig_Simple();

In the MCANConfig_Simple() function, I referred to the project examples(mcan_ex7_classic_transmit.c) of CPU1 that configured the MCAN to classic CAN. The bit time settings are listed as follows:    //
    // Initialize bit timings.
    bitTimes.nomRatePrescalar   =0x3U; // Nominal Baud Rate Pre-scaler.
    bitTimes.nomTimeSeg1        =0x9U; // Nominal Time segment before SP.
    bitTimes.nomTimeSeg2        =0x8U; // Nominal Time segment after SP.
    bitTimes.nomSynchJumpWidth  =0x8U; // Nominal SJW Range.

However, It doesn't work. I guess that the baud rate of the MCAN is not configured properly, however, I can not find some useful references.

So  please help me about the use of MCAN as classic CAN in Cortex-A4.

And aso I want to ask that if MCAN is configured to CANFD, if the CAN monitor card must support the CANFD communication? 

Thank you very much !