This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: 我使用epwm触发多个soc转换单通道,但此时的采样率不能更改

Part Number: TMS320F28379D

#include "Includes.h"
#include "RFFT.h"
//adc.h ADC_RESOLUTION_xBIT 重复定义

#define RESULTS_BUFFER_SIZE     2048
#define EX_ADC_RESOLUTION       12
//
#pragma DATA_SECTION(FFT_input, "ramgs0")
uint16_t FFT_input[RESULTS_BUFFER_SIZE];
uint16_t periodCount;         //采样率=100M/((periodCount-1)+1)
volatile uint16_t bufferFull;                // Flag to indicate buffer is full


extern RFFT_Analyse_Struct rfft_analyse;


void initADC(void);
void initEPWM(void);
void initADCSOC(void);
__interrupt void adcA1ISR(void);
void LED_Init(void);
void configureDMAChannels(void);
void initializeDMA(void);
__interrupt void dmach1ISR(void);

void main(void)
{
//确定运行模式,使用CPU2
#ifdef _STANDALONE
#ifdef _FLASH

    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
#else

    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
#endif
#endif

   //设备初始化
    Device_init();
    //GPIO初始化
    Device_initGPIO();

    Interrupt_initModule();
    Interrupt_initVectorTable();

    Interrupt_register(INT_ADCA1, &adcA1ISR);
    Interrupt_register(INT_DMA_CH1, &dmach1ISR);

    periodCount=50;

    initADC();
    initEPWM();
    initADCSOC();

    LED_Init();
    SCI_A_Init(115200);

    for(int index = 0; index < RESULTS_BUFFER_SIZE; index++)
        {
        FFT_input[index] = 0;
        }
        bufferFull = 0;


        Interrupt_enable(INT_ADCA1);
        Interrupt_enable(INT_DMA_CH1);

        initializeDMA();
        configureDMAChannels();

        DMA_clearTriggerFlag(DMA_CH1_BASE);   // DMA channel 1

    //开启总中断
    Interrupt_enableMaster();

        DMA_startChannel(DMA_CH1_BASE);
        EPWM_enableADCTrigger(EPWM1_BASE, EPWM_SOC_A);
        EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_UP);

        while(bufferFull == 0)
        {
        }
        bufferFull = 0;

//            RFFT_ADC_Init();
       for(int index = 0; index < RESULTS_BUFFER_SIZE; index++)
            micro_print(SCIA_BASE,"signal:%d\n",FFT_input[index]);

//                    RFFT_ADC_Caculate();

    while(1)
    {
        NOP;
    }
}

void LED_Init(void)
{
    GPIO_setPinConfig(DEVICE_GPIO_CFG_LED1);
    GPIO_setMasterCore(DEVICE_GPIO_PIN_LED1, GPIO_CORE_CPU1);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_LED1, GPIO_PIN_TYPE_STD);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_LED1, GPIO_DIR_MODE_OUT);
    GPIO_WritePin(DEVICE_GPIO_PIN_LED1, 1);
    GPIO_setPinConfig(DEVICE_GPIO_CFG_LED2);
    GPIO_setMasterCore(DEVICE_GPIO_PIN_LED2, GPIO_CORE_CPU1);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_LED2, GPIO_PIN_TYPE_STD);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_LED2, GPIO_DIR_MODE_OUT);
    GPIO_WritePin(DEVICE_GPIO_PIN_LED2, 1);
}

void initADC(void)
{
    ADC_setPrescaler(ADCA_BASE, ADC_CLK_DIV_4_0);

#if(EX_ADC_RESOLUTION == 12)
    ADC_setMode(ADCA_BASE, ADC_RESOLUTION_12BIT_0x00U, ADC_MODE_SINGLE_ENDED);//ADC_RESOLUTION_12BIT_0x00U
#elif(EX_ADC_RESOLUTION == 16)
    ADC_setMode(ADCA_BASE, ADC_RESOLUTION_16BIT_0x40U, ADC_MODE_DIFFERENTIAL);
#endif

    ADC_setInterruptPulseMode(ADCA_BASE, ADC_PULSE_END_OF_CONV);

    ADC_enableConverter(ADCA_BASE);
    DEVICE_DELAY_US(1000);
}


void initEPWM(void)
{
    EPWM_disableADCTrigger(EPWM1_BASE, EPWM_SOC_A);


    EPWM_setADCTriggerSource(EPWM1_BASE, EPWM_SOC_A, EPWM_SOC_TBCTR_U_CMPA);
    EPWM_setADCTriggerEventPrescale(EPWM1_BASE, EPWM_SOC_A, 1);


    EPWM_setCounterCompareValue(EPWM1_BASE, EPWM_COUNTER_COMPARE_A, 10);
    EPWM_setTimeBasePeriod(EPWM1_BASE, periodCount-1);


    EPWM_setClockPrescaler(EPWM1_BASE,
                           EPWM_CLOCK_DIVIDER_1,
                           EPWM_HSCLOCK_DIVIDER_1);

    EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_STOP_FREEZE);
}


void initADCSOC(void)
{
    uint32_t adcBase = ADCA_BASE;
    uint16_t channel = ADC_CH_ADCIN0;
    uint16_t acqps;
#if(EX_ADC_RESOLUTION == 12)
    acqps = 15;
#elif(EX_ADC_RESOLUTION == 16)
    acqps = 64;
#endif

        // Configure SOCs channel no. & acquisition window.
        // Trigger SCO0 from EPWM2SOCA.
        // Trigger all other SOCs from INT1 (EOC on SOC0).
        //
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER0, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER1, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER2, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER3, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER4, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER5, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER6, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER7, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER8, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER9, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER10, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER11, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER12, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER13, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER14, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);
        ADC_setupSOC(adcBase, ADC_SOC_NUMBER15, ADC_TRIGGER_EPWM1_SOCA,
                     (ADC_Channel)channel, acqps);

    ADC_setInterruptSource(ADCA_BASE, ADC_INT_NUMBER1, ADC_SOC_NUMBER15);
    ADC_enableInterrupt(ADCA_BASE, ADC_INT_NUMBER1);
    ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
}

__interrupt void adcA1ISR(void)
{
    ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);

    //
    // Check if overflow has occurred
    //
    if(true == ADC_getInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1))
    {
        ADC_clearInterruptOverflowStatus(ADCA_BASE, ADC_INT_NUMBER1);
        ADC_clearInterruptStatus(ADCA_BASE, ADC_INT_NUMBER1);
    }

    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1);
}

__interrupt void dmach1ISR(void)
{
    bufferFull = 1;
    EPWM_disableADCTrigger(EPWM1_BASE, EPWM_SOC_A);
    EPWM_setTimeBaseCounterMode(EPWM1_BASE, EPWM_COUNTER_MODE_STOP_FREEZE);

    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP7);
}

void initializeDMA(void)
{
    DMA_initController();
    DMA_setEmulationMode(DMA_EMULATION_FREE_RUN);
}


void configureDMAChannels(void)
{
    DMA_configAddresses(DMA_CH1_BASE, (uint16_t *)&FFT_input,
                        (uint16_t *)ADCARESULT_BASE);

    DMA_configBurst(DMA_CH1_BASE, 16, 2, 2);
    DMA_configTransfer(DMA_CH1_BASE, (RESULTS_BUFFER_SIZE >> 4), -14, 2);
    DMA_configMode(DMA_CH1_BASE, DMA_TRIGGER_ADCA1,
                   (DMA_CFG_ONESHOT_DISABLE | DMA_CFG_CONTINUOUS_DISABLE |
                    DMA_CFG_SIZE_32BIT));

    DMA_enableTrigger(DMA_CH1_BASE);
    DMA_disableOverrunInterrupt(DMA_CH1_BASE);
    DMA_setInterruptMode(DMA_CH1_BASE, DMA_INT_AT_END);
    DMA_enableInterrupt(DMA_CH1_BASE);

}