This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MCU SPI能输出时钟信号,SOMI能接收外部输入信号,但是SIMO无输出信号,一直为0
IO映射:
RESET :GPIO56
DRDY :GPIO27
SCLK :GPIO26
SOMI :GPIO31
SIMO :GPIO30
SPI从设备为ads131m06,不管mcu发出什么数据,SIMO上捕获到的数据总是0.
将GPIO30配置为普通IO,可以控制其高低电平。
请帮忙看看是哪里出了问题
初始化SPI代码:
void SPI_Initialize(void) { SpibRegs.SPICCR.bit.SPISWRESET = 0; //spi reset to configuration mode SpibRegs.SPICCR.bit.CLKPOLARITY = 0; //DOut on falling Edge,Din on rising Edge SpibRegs.SPICCR.bit.SPICHAR = (8-1); //16-bit word SpibRegs.SPICCR.bit.SPILBK = 0; //loopback disabled SpibRegs.SPICTL.bit.MASTER_SLAVE = 1; //Master SpibRegs.SPICTL.bit.TALK = 1; //Transmit Enable SpibRegs.SPICTL.bit.CLK_PHASE = 0; //normal clocking scheme,no delaying SpibRegs.SPICTL.bit.SPIINTENA = 0; //Interrupt Disable SpibRegs.SPIBRR.bit.SPI_BIT_RATE = SPI_BRR; //500kbps SpibRegs.SPIPRI.bit.FREE = 1; //Halting on a breakpoint will not halt the SPI DELAY_US(10); //b15,SPIRST =1,resume FIFO to transmit or receive //b14,SPIFFENA =1,enable FIFO //b13,TXFIFO =1,release TX FIFO from reset //b6,TXFFINTCLR =1,clear SPIFFTX[TXFFINT] flag //b4~b0,TXFFIL =4,generate TX FIFO interrupt when there are less than 4 words in TX buffer SpibRegs.SPIFFTX.all = 0xE040; //b13,RXFIFORESET=1,re-enable RXFIFO //b6,RXFFINTCLR =1,clear SPIFFRX[RXFFINT] flag //b4-b0,RXFFIL = F,generate RX FIFO intterupt when there are more than 15 words in RX buffer SpibRegs.SPIFFRX.all = 0x204F; //no delay between every transfer from FIFO transmit buffer to transmit shift register SpibRegs.SPIFFCT.all = 0x0; SpibRegs.SPICCR.bit.SPISWRESET = 1; //Release the SPI from reset SPI_InitGpio(); } // // InitSpiGpio - Initialize SPIA GPIOs // void SPI_InitGpio() { EALLOW; GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0; // Enable pull-up (SPISIMO) GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0; // Enable pull-up (SPISOMI) GpioCtrlRegs.GPAPUD.bit.GPIO26 = 0; // Enable pull-up (SPICLK) GpioCtrlRegs.GPAPUD.bit.GPIO27 = 0; // Enable pull-up (SPISTE) GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3; // Asynch input (SPISIMO) GpioCtrlRegs.GPAQSEL2.bit.GPIO31 = 3; // Asynch input (SPISOMI) GpioCtrlRegs.GPAQSEL2.bit.GPIO26 = 3; // Asynch input (SPICLK) GpioCtrlRegs.GPAQSEL2.bit.GPIO27 = 3; // Asynch input (SPISTE) GpioCtrlRegs.GPAGMUX2.bit.GPIO30 = 0; //0x3 GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 3; //SPIB_SIMO GpioCtrlRegs.GPAGMUX2.bit.GPIO31 = 0; //0x3 GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 3; //SPIB_SOMI GpioCtrlRegs.GPAGMUX2.bit.GPIO26 = 1; //0x6 GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 2; //SPIB_CLK GpioCtrlRegs.GPAGMUX2.bit.GPIO27 = 0; // GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 0; // GpioCtrlRegs.GPADIR.bit.GPIO27 = 0; // Input GpioCtrlRegs.GPAPUD.bit.GPIO27 = 0; // Enable pull-up /DRDY GpioCtrlRegs.GPACTRL.bit.QUALPRD3= 0x3;//6 SYSCLK cycles GpioCtrlRegs.GPBGMUX2.bit.GPIO56 = 0; GpioCtrlRegs.GPBMUX2.bit.GPIO56 = 0; GpioCtrlRegs.GPBPUD.bit.GPIO56 = 0; // Enable pull-up (SPI /RESET) GpioCtrlRegs.GPBDIR.bit.GPIO56 = 1; // Output GpioDataRegs.GPBSET.bit.GPIO56 = 1; // High // GpioDataRegs.GPBCLEAR.bit.GPIO56 = 1; // Low,保持复位状态 //GpioCtrlRegs.GPAGMUX2.bit.GPIO30 = 0; //0 //GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 0; //GPIO30 //GpioCtrlRegs.GPADIR.bit.GPIO30 = 1; // Output EDIS; }
内容重复,我会关闭这个帖子。工程师将在下帖中跟进您的问题:
https://e2echina.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/757646/tms320f280049-spib-simo