Part Number: TMS320F28377S
请问TMS320F28377S内部配置上拉时候,上拉电阻是多大?ADC输入的电压耐受范围是多少,是否可以承受5V输入不损坏器件?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28377S
请问TMS320F28377S内部配置上拉时候,上拉电阻是多大?ADC输入的电压耐受范围是多少,是否可以承受5V输入不损坏器件?
TMS320F28377S内部配置上拉时候,上拉电阻是多大?
数据手册上没有的就是没有。但有电流数据供参考:

ADC输入的电压耐受范围是多少
0~2.5V或者0~3V,取决于参考电压的选择;最大不能超过3.3V;
是否可以承受5V输入不损坏器件?
不可以。