Part Number: TMS320F28377D
Other Parts Discussed in Thread: CONTROLSUITE
28377的引脚上电前配置成SCI boot,GPIO72=0、GPIO84=1,用到的文件serial_flash_programmer.exe、F2837xD_sci_flash_kernels_cpu01.txt、F2837xD_sci_flash_kernels_cpu02.txt、Longgang_TCUcontrolCPU1_230227.txt、Longgang_TCUcontrolCPU2_230227.txt放在同一路径,用的USB转串口线连接,上电进入CMD运行“serial_flash_programmer.exe -d f2837xD -k F2837xD_sci_flash_kernels_cpu01.txt -a Longgang_TCUcontrolCPU1_230227.txt -m F2837xD_sci_flash_kernels_cpu02.txt -n Longgang_TCUcontrolCPU2_230227.txt -b 9600 -v -p COM2”后停留在“Attempting autobaud to load kernel...”,使用串口端口配置无误,请问是什么原因了?用的z-tek力特工业级USB转串口线RS485/422转换器
。
还有,是否有关于用CMD运行serial_flash_programmer下载DSP程序过程中出现的异常情况汇总说明啊?
DSP确认进入了SCI boot 模式,接收引脚GPIO85用示波器测到了第一个字节波形(查看资料第一字节信息是0xAA?)


这个工程生成2ms间隔发送一个字的serial_flash_programmer.exe ?把15ms这个间隔(如下图)缩短至2ms左右是否可实现?因为没用过VS开发,不会研究开发这个
,蓝绿--DSP SCI 接收引脚,黄色--DSP SCI 发送引脚。示波器设置的2ms一格,这里显示两次接收间隔约为15ms,波特率用的38400bps