This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用的是TMS320F28035芯片,在烧录程序的时候经常会出现low-power mode的错误提示,无法烧录。经检测dsp供电正常,仿真器也没有问题。还有可能是什么问题.
错误提示如下:
Trouble Reading FP Register:
(Error -1156 @ 0x1)
Device may be operating in low-power mode. Do you want to bring it out of this mode?
(Emulation package 5.0.681.0)
console:
C28xx: Flash Programmer: Warning: The configured device (TMS320F28035), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: Trouble Reading FP Register: (Error -1156 @ 0x1) Device may be operating in low-power mode. Do you want to bring it out of this mode? (Emulation package 5.0.681.0)
C28xx: GEL Output:
Device Calibration not complete, check if device is unlocked and recalibrate.C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Warning: Target was left running after a reset during a Flash operation.
C28xx: Warning: Target was left running after a reset during a Flash operation.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: GEL Output:
Device Calibration not complete, check if device is unlocked and recalibrate.
请各位帮帮忙