This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D的input x-bar 和output x-bar 问题



这款芯片新增的input x-bar 和output x-bar 功能

我能不能这么理解这两个功能:

1.output x-bar可以将DSP内部的一些信号引出到任意一个GPIO口上

2.input x-bar可以将任意一个GPIO口的信号,引到DSP内部,比如任何一个GPIO口的信号,都可以配制成EPWM模块的TZ信号