This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

逆变器F28335 PWM出口关断问题



       公司使用了F28335芯片开发逆变器,应用了EPWM1A/B、EPWM2A/B、EPWM4A/B六路PWM。当出现异常保护时,现采用的处理方式是先将六路PWM口模式改为GPIO口模式,然后再将出口数据置零,经试验不可靠,六路输出不能都同时置为低电平,有1到2路仍为高电平的情况出现,严重时出现IGBT直通而烧坏管子。烦请TI专家和各位高手帮忙参考一下,并提供可行的解决方案,先行谢过啦!参考程序如下:

/*PWM端口数据宏定义*/

#define  PWM_AL    GpioDataRegs.GPADAT.bit.GPIO1  
#define  PWM_AH   GpioDataRegs.GPADAT.bit.GPIO0 
#define  PWM_BL   GpioDataRegs.GPADAT.bit.GPIO3 
#define  PWM_BH   GpioDataRegs.GPADAT.bit.GPIO2 
#define  PWM_CL   GpioDataRegs.GPADAT.bit.GPIO7 
#define  PWM_CH  GpioDataRegs.GPADAT.bit.GPIO6

逆变器异常保护时如下处理:

/* PWM 模式设置为GPIO */

EALLOW;
GpioCtrlRegs.GPAMUX1.bit.GPIO0 = 0;   // GPIO0 = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO1 = 0;   // GPIO1 = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO2 = 0;   // GPIO2 = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 0;   // GPIO3 = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0;   // GPIO6 = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 0;   // GPIO7 = GPIO
EDIS;

/* PWM口清零关断 */
PWM_AH=0;
PWM_BH=0;
PWM_CH=0;

PWM_AL=0;
PWM_BL=0;
PWM_CL=0;