This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问TI专家:C2000的耐温与抗干扰问题



我们专做汽车电机控制器,行业标准要求把MCU板和功率板一起密封在一个刚好能容纳的金属容器中,容器内的温度可达90摄氏度,

请问TI的C2000系列MCU能否在这种环境中长时间运行吗?

       因为mcu板贴近功率板有干扰,c2000能否稳定运行吗?

现在我们用microchip,耐温有问题,抗干扰成本较高。

      我们做的是超低成本产品,TI有没有合适的解决方案?

  • C2000有汽车级的芯片,它支持-40~125度环境温度,结点温度要求小于150度。

    至于抗干扰,对于C2000芯片而言只要能保证时钟和电源的供给稳定就能正常圆形,部分C2000芯片有内置的震荡器,所以只要供电能够保证稳定那C2000芯片就能稳定运行。

    您可以考虑有内置的震荡器的TI2802x或2803x系列芯片,然后参考TI的controlcard的PCB设计。

    www.ti.com/.../tms320f28027

    www.ti.com/.../tms320f28035

  • 标称同样温度等级芯片,当芯片背面pcb板面温度达92度(此时环境温度80度左右)开始有不稳定现象,在这种情况下,ti产品能表现好点吗?

    你推荐的28027(28035)与28065比,除价格外,有何不同?28065多了点东西功耗是否也大?(实用层面,芯片自身温度是否也高些?)

  • TI的产品只要在datasheet的要求环境下就能正常运行。请看datasheet的Electrical Specifications章节

    至于功耗,这和使用了哪些片上模块有关系,如果是用一样的模块,在一样的频率下运行,那他们的功耗基本一致。具体的可以看一下2个芯片的datasheet中的Current Consumption章节。