This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280038C-Q1: 外部晶振不起振

Part Number: TMS320F280038C-Q1

Hi,

目前使用TMS320F280038C-Q1使用外部晶振,不起振,请帮忙看下

  • 最大驱动电平大于1mW是什么意思,我看几乎没有晶振可以满足

  • 有通过XCLKOUT查看XTAL的波形吗?

    从C2000器件的角度讲,最大驱动电平是指C2000器件内部的电子振荡器提供给外部晶体的最大驱动功率;外部晶体的最大驱动能力是指外部晶体所能耗散的最大驱动功率。根据提供的晶体的规格书来看,0.2mW是小于1mW的,所以应该增加阻尼电阻Rd;

    最大驱动电平大于1mW是什么意思,我看几乎没有晶振可以满足

    这个观点我认同,我得去和相关的工程师再确认一下。阻尼电阻也是放在最后来调的。

    根据规格书中给出的Rr、C0、CL,结合F280038C datasheet第93页给出的公式,可以算出ESR = 78.125Ω;而原理图中,CL1 = CL2 = 8pF,CL = 4pF,ESR = 112.5Ω,都是达不到ESR <= 50Ω的要求的;

    综上,首先把CL1以及CL2换成16pF的,这样串联后的CL才是8pF,符合晶体以及F280038C的要求;其次,关于ESR,如果不考虑C0作用的话,ESR = Rr = 50Ω,也是满足要求的。

    所以先把两个负载电容换掉试一下。