尊敬的TI专家们:
我在工程中设置了ADC为16位差分输入模式,但是结果寄存器中数值仍为12位。根据
帖子的描述,我检查了DevCfgRegs.PERCNF1_1寄存器,发现其4个ADC_MODE位为1,因此无法启用16位模式。我根据上述帖子的步骤将该寄存器复位,启用ADC的16bit模式成功,但是重新上电时该寄存器又变为1.

我的问题是:1.该帖子中提到的是”较早的TMX型号“,但我使用的是TMS系列,且商家说他们这批芯片不是很老。请问现在的芯片还有这个问题吗?有没有办法不需要每次上电都重新配置这个寄存器?
2.该帖子中说”so performance will not meet datasheet specifications“,在我启用ADC的16bit模式后,没有输入的RC滤波,其在500ns采样窗口下测量板载的经缓冲的REF5030分压后电压,转换值跳动达到了10LSB(p-p),请问正常应该是多少?在我的电路中出现这么大的跳动主要原因是芯片问题还是我的硬件设计问题?